alert icon

Internet Explorer 8 or 9 is not supported by this website. Please use a more up to date browser.

Hide Message hide icon

FAQs: How to Avoid Hydrogen Embrittlement

Swagelok hydrogen embrittlement materials selection

FAQs: How to Avoid Hydrogen Embrittlement and Other Hydrogen Handling Issues

Buddy Damm, Senior Scientist, Swagelok

Graphic of hydrogen production, from production to transportation to use.Independence from fossil fuels. An energy crisis resulting from geopolitical conflict. The increasing urgency to confront climate change. These are just a few of the reasons driving the search for viable alternative fuels.

Hydrogen is one promising solution. Handling hydrogen safely and reliably, from generation to end use, is the key to reaching its fullest potential as a zero-emission fuel source in a wide variety of applications.

However, containing and transferring hydrogen presents some unique challenges. Hydrogen is the first element in the periodic table, consisting of a single positively charged proton and a single negatively charged electron. It is the lightest and among the smallest of atoms. In the developing hydrogen economy, hydrogen will need to be handled in liquid form and gaseous form. Hydrogen liquifies at −252.9°C (−423°F) and is about 140 times denser as a liquid compared to the gaseous form. Transporting and storing H2 as a liquid is more efficient, but at its point of use, H2 is a gas. As a result, two phenomena can impact metals used in hydrogen systems.

  1. Low-temperature embrittlement: As temperature decreases, metals lose some ductility.
  2. Hydrogen embrittlement: At higher temperatures where hydrogen is a gas, atomic hydrogen can diffuse into the metal and cause embrittlement.

Here, embrittlement refers to a reduction in a metal’s ductility and resistance to fracture and fatigue in its service environment compared to its resistance to fracture and fatigue in air and at room temperature. These issues can lead to system failure, resulting in safety risks, increased downtime, and financial loss. As the hydrogen industry continues to expand, addressing these system construction challenges is critical to the fuel’s widespread adoption as a long-term, sustainable fuel solution.

Learn About Hydrogen Facts At-A-Glance

So, how can hydrogen professionals build hydrogen handling systems that last? It is critical to remember that materials matter for hydrogen containment. Fluid systems made with specifically formulated, high-quality stainless steel can better resist the challenges inherent to hydrogen containment. The following FAQs will explain how and what specifiers should be considering in their materials selection for hydrogen containment components.

Chart demonstrating the effect of temperature on embrittlement in different types of stainless steel

Q: What is low-temperature embrittlement?

A: Low-temperature embrittlement refers to a reduction in ductility, toughness, or fatigue and fracture resistance as the temperature is decreased. Austenitic stainless steels suffer only minor, low-temperature embrittlement while ferritic steels (low-alloy steels and ferritic stainless steels) are more susceptible. For this reason, austenitic stainless steels are the gold standard for liquid hydrogen systems.


Diagram of hydrogen molecules dissociating to atomic hydrogen and penetrating a metal

Q: How does hydrogen penetrate metals?

A: Hydrogen molecules (H2, blue) can dissociate to atomic hydrogen (H, red) and penetrate a metal. Hydrogen atoms accumulate at stress concentrations such as crack tips or microstructural features like grain boundaries, inclusions, or precipitates. In certain cases, atomic hydrogen can reform as diatomic hydrogen.

Q: What is hydrogen embrittlement?

A: Hydrogen embrittlement causes a reduction in fatigue and fracture resistance of a metal. Very high-strength materials experience more severe hydrogen embrittlement.Hydrogen embrittlement causes a reduction in fatigue and fracture resistance of a metal
 

While stainless steels are generally more compatible with hydrogen than many other metals, not all resist hydrogen embrittlement equally.

 

Austenitic stainless steels are characterized by their face center cubic (FCC) crystal structure, moderate strength and naturally high ductility. And while they are generally more compatible with hydrogen than many other metals, not all resist hydrogen embrittlement equally.

Q: What are the potential consequences of using more susceptible stainless steel?

A: Choosing materials that are more susceptible to hydrogen embrittlement can lead to a greater likelihood of a failure in system integrity.

Fatigue capability reduction is a greater concern than ductility loss. Ductility refers to the degree to which the material can sustain plastic deformation under tensile stress before failure. Appropriately designed components are not subjected to stresses that result in macroscopic plastic deformation. Instead, cyclic loading due to pressure cycling, vibration, or other service loading can result in slowly accumulated localized plastic damage and failure due to fatigue—the weakening of the steel due to repeated stresses or loadings. System or component failure potential may become further exacerbated if materials are subject to corrosive environmental factors.

Component failure, of course, can lead to a number of undesirable outcomes, including:

Graph demonstrating benefits of nickel content in combating hydrogen embrittlement.
Ferritic alloys with very low nickel content become significantly embrittled, while austenitic alloys between 10% and 30% nickel show relatively little embrittlement.
  • Potential safety issues
  • Excessive downtime for maintenance or repair
  • More frequent component replacement
  • Sustainability concerns due to hydrogen escaping into the environment
  • Higher total cost of operation and ownership for the asset
  •  

    Q: How can I differentiate higher-quality stainless steels versus lower ones?

    A: High-quality stainless steels containing elevated levels of nickel have been shown to be better suited to handle H2—particularly over a long service life.

    The American Society for Testing and Materials (ASTM) requires a minimum of 10% nickel in 316 stainless steel formulations, but 316 stainless steel with a minimum of 12% nickel is better for the unique challenges posed by hydrogen. Nickel content helps stabilize the microstructure of stainless steel, enabling it to be more resistant to hydrogen embrittlement. In our testing, we have found hydrogen embrittlement’s effect on tensile ductility in 316 stainless steel with 12% Ni was found to be minor.Material Science icon

    316 stainless steel with a minimum of 12% nickel is better suited for the unique challenges of hydrogen.



    Chart demonstrating higher nickel content in Swagelok 316 stainless steel.
    Stainless steel with higher levels of nickel content can help prevent hydrogen embrittlement.

    A: While 316 stainless steel with high nickel content is generally a compelling choice for hydrogen system construction, there may be situations where performance criteria for a specific application, such as a need to prioritize material strength or corrosion resistance, make another material choice a good option. Proper system design and maintenance can help deter embrittlement in these cases. Organizations like Swagelok continue to research and understand the impact of hydrogen on other alloys and can help you make informed decisions.

    Q: How can I be sure I am selecting high-performance materials?

    It can be challenging to discern which materials are optimal for different fluid handling applications, particularly in the burgeoning hydrogen industry. But it is important to get it right. There are long-term implications for specifying materials for hydrogen handling systems. Most importantly, the wrong choices have the potential to damage hydrogen’s reputation as a reliable and viable fuel source for a cleaner future.

    Seek out suppliers that can demonstrate a thorough understanding of materials science and have developed products successfully used in hydrogen applications. If you need assistance, Swagelok’s hydrogen specialists are happy to help you select optimal materials for your application and find a solution that meets your needs.

    Two hydrogen specialists consulting to select optimal materials for hydrogen applications

    Explore Clean Energy Solutions

    Related Articles

    Select the right hydrogen valves for your application

    What to Look for in Hydrogen Valves

    Valves are critical parts of hydrogen fluid systems. Learn what to look for in an ideal hydrogen valve and how it can contribute to safer, more reliable hydrogen transportation.

    Hydrogen Fuel Cell Technology

    The Anatomy of a Hydrogen Fitting

    Learn why fittings designed specifically for hydrogen applications can help fuel cell vehicle OEMs and infrastructure developers achieve safer and more reliable fuel systems.

    Hydrogen measurement and control

    Measuring and Controlling Hydrogen Flow

    See how an automotive testing and simulation company partnered with Swagelok to transition to hydrogen fuels technology.